Implement security

FactoryTalk
e
Procedure
takes advantage of the security features of
FactoryTalk Batch View
. [See the for more information.]
The logged in user should:
  • be an
    FactoryTalk
    Security user or a Windows-linked user
  • be a user with rights to all of the buttons
If operators wish to perform a function that is secured, for instance
Abort
, they must enter a user name and password, which is checked against the
FactoryTalk
Security settings defined in the
FactoryTalk
Directory. [See the for more information.]
IMPORTANT:
FactoryTalk
Security cannot be used to secure
e
Procedure
instructions. However, instructions can be secured through verification signatures.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal