FactoryTalk Batch Client security
FactoryTalk Batch
Client securityFactoryTalk Batch
View, FactoryTalk
e
ProcedureFactoryTalk Batch View HMI Controls
, Equipment Editor, and Recipe
Editor use FactoryTalk
Security, which allows security settings to be shared
among FactoryTalk
enabled products across a network or on the same computer.
FactoryTalk
Directory is the infrastructure which contains the security
policies defined for FactoryTalk
Security secured resources.FactoryTalk Batch
secured resources include Batch Commands, Phase Commands, the
Batch View windows, and log ons to FactoryTalk Batch
components. For a complete
list of FactoryTalk Batch
secured objects and their default security policy
settings, refer to the FactoryTalk Batch
Administrator's User Manual
, publication BATCH-UM003
FactoryTalk Batch
product policies are created in the Network Directory when the
FactoryTalk® Services Platform
installs. The FactoryTalk Batch
product polices
are used to restrict access to the FactoryTalk Batch
client components and the
features within them. (See the FactoryTalk
Help for more information.)The
FactoryTalk Services Platform
Services Platform installation process:- Creates both aWhen the install process finishes, both directories are fully configured and ready for use.FactoryTalkLocal Directory and aFactoryTalkNetwork Directory on the computer.TIP:Security settings are completely separate in the Network Directory and Local Directory. Changes you make to the security settings in the Network Directory do not affect the Local Directory and vice versa.
- Allows any Windows Administrator user account to log on to either directory.The installation process automatically adds the local Windows Administrators group to theFactoryTalkAdministrators group in eachFactoryTalkDirectory.
- Allows any authenticated Windows user to log on to theThe installation process automatically adds all members of the local Windows Authenticated Users group to theFactoryTalkLocal Directory.FactoryTalkLocal Directory.
- Allows all new user accounts full access permissions.The installation process automatically sets system policies to allow all new user accounts added to either directory full access to that directory by default.
Provide Feedback