FactoryTalk Batch View security
Security for the .
FactoryTalk Batch View
is implemented using the FactoryTalk
Security product policy settings defined in the FactoryTalk Directory
. The system administrator must configure FactoryTalk
Security prior to using the FactoryTalk Batch View
. Instructions for configuring security are in the FactoryTalk Batch
Administrator's User Manual, publication BATCH-UM003Any
FactoryTalk
Security user with the appropriate permissions can log on or off of the FactoryTalk Batch View
. The FactoryTalk Batch View
can be configured to require user authentication each time a command is issued. Users can
log on or off of the FactoryTalk Batch View
without stopping or exiting ANY application. The FactoryTalk Batch View
security can automatically log off the current user if the FactoryTalk Batch View
is inactive for a period of time. Commands sent to the FactoryTalk Batch
Server from the FactoryTalk Batch View
are logged in the electronic batch record along with the name of the user who initiated
the command. Provide Feedback