Configure the
e
Procedure
service

The
e
Procedure
Service is installed on the
FactoryTalk Batch
Server computer and requires no special configuration. The
e
Procedure
Service can be configured to start manually by changing the startup type in the
Services
dialog box of the Control Panel. [See the for more information.]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal