Add the Batch Server user account to the client computer
If the Batch Server user account is a workgroup account or if the for more information.)
FactoryTalk Batch
Server computer needs to access files on the client computer, you must add the Batch
Server user account to all FactoryTalk Batch
client computers. (See the FactoryTalk Batch
Administrator's User
Manual, publication BATCH-UM003Provide Feedback