Recipe execution requests

Use the PXRQ instruction in the phase logic to request these types of data available or meaningful only during Batch execution:
  • Download
    Material Manager
    Data Container in Use
  • Upload
    Material Manager
    Data Container in Use
  • Download Container Binding Priority
  • Upload Container Binding Priority
  • Download Sufficient Material
These commands give the phase logic programmer access to the data of the material entities the phase logic interacts with.
The attribute ID for a standard attribute is the index. The attribute ID for a custom attribute is the sum of the controller ID and the index.
Summary of these recipe execution requests:
Summary of recipe execution requests
External Request
DINT[0]
DINT[1]
DINT[2]
Description
Download
Material Manager
Data Container in Use
1
Attribute ID
Array Index
Download data about the container currently in use.
Download
Material Manager
Data Container in Use
2
Attribute ID
Array Index
Download data about the current material inside the container currently in use.
Download
Material Manager
Data Container in Use
3
Attribute ID
Array Index
Download data about the current lot inside the container currently in use.
Upload
Material Manager
Data Container in Use
1
Attribute ID
Array Index
Upload data about the container currently in use.
Upload
Material Manager
Data Container in Use
2
Attribute ID
Array Index
Upload data about the current material inside the container currently in use
Upload
Material Manager
Data Container in Use
3
Attribute ID
Array Index
Upload data about the current lot inside the container currently in use.
Download Container Binding Priority
Array Index
Download the current binding's container priority
Upload Container Binding Priority
Array Index
Upload a new container priority for the current binding.
Download Sufficient Material
Array Index
Download data about sufficient material for step.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal