Download selection for current binding

Configure the PXRQ instruction in
Logix Designer
to download the container selection priority for the material, container, feed type, and unit currently in use by this phase.
PXRQ instruction configuration
External Request
Data Value Array Element
Value
Download Container Binding Priority
DINT[0]
Phase parameter tag number.
DINT[1]
DINT[2]
The value is stored into a specified tag.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal