Upload data into container in use

This request fails (without notice) if the data is read-only.
Configure the PXRQ instruction in
Logix Designer
to upload material data about the current material inside the container the phase currently runs against.
PXRQ instruction configuration
External Request
Data Value Array Element
Value
Upload
Material Manager
Data Container in Use
DINT[0]
2
DINT[1]
Data to upload into.
DINT[2]
Report tag address of the value stored in the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal