Upload data to container in use

This request fails (without notice) if the data is read-only
Configure the PXRQ instruction to upload container data about the container the phase is currently running against.
PXRQ instruction configuration
External Request
Data Value Array Element
Value
Download
Material Manager
Data Container in Use
DINT[0]
1
DINT[1]
Data to upload into (attribute ID).
DINT[2]
Report tag address of the value stored in the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal