FactoryTalk Batch Services Properties dialog—Descriptors and Defaults tab

In the
FactoryTalk Batch Services Properties
dialog, use the
Descriptors and Defaults
tab to configure Cross Invocation strings and hyperlinks.

Cross Invocation descriptors and defaults

Cross Invocation is the means by which
FactoryTalk® Batch View
HMI Controls passes data to, and activates, an automation server such as an HMI or Visual Basic program. The data is specific to an equipment resource type within an area model.
Each time a selection changes in
FactoryTalk Batch View
and HMI Controls, the system retrieves the Cross Invocation strings associated with the equipment resource from the
FactoryTalk Batch
Server and evaluates them.
You can define up to five Cross Invocation strings per resource type.
Cross Invocation settings
Setting
Description
Resource types
Shows the resource type for the Cross Invocation strings that you define. Select one of the following from the list:
  • Phase
  • Process Cell
  • Resource
  • Unit
Descriptors
Shows the Cross Invocation string labels for the selected resource type. These labels appear in
FactoryTalk Batch Equipment Editor
(
Edit Properties dialog
Cross Invocation tab
).
This field has a maximum length of 128 characters.
Default values
Shows the default Cross Invocation string values for the selected resource type. Information in the string can include a shortcut menu item and subitems, the caption for a shortcut menu item, and the data to pass to the automation server.
The label in
Descriptors
box
1
corresponds to the Cross Invocation string in
Default values
box
1
.
This field has a maximum length of 128 characters.

Hyperlink descriptors and defaults

Hyperlinks are the means by which
FactoryTalk Batch View
can map equipment to the appropriate
FactoryTalk Batch View
directory.
TIP: The
Hyperlink descriptors and defaults
area is only accessible if, from the
General
tab, you selected the
Enable FactoryTalk eProcedure
option. Refer to the for more hyperlink information.
You can define up to five hyperlinks per resource type.
Hyperlink settings
Setting
Description
Resource types
Shows the resource type for the hyperlinks that you define. Select one of the following from the list:
  • Phase
  • Process Cell
  • Resource
  • Unit
Descriptors
Shows the hyperlink URL labels for the selected resource type. These labels appear in
FactoryTalk Batch Equipment Editor
(
Edit Properties dialog
Hyperlink tab
).
This field has a maximum length of 128 characters.
Default values
Shows the default hyperlink URLs for the selected resource type. The label in
Descriptors
box
1
corresponds to the URL in
Default values
box
1
.
This field has a maximum length of 128 characters.
TIP:
If a hyperlink value is not defined, either as a default or when you create the specific resource type instance, the hyperlink label is not visible in
e
Procedure
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal