Hyperlink descriptors and defaults

Hyperlinks are the means by which
FactoryTalk® Batch View
can map equipment to the appropriate
FactoryTalk Batch View
directory. If a hyperlink value is not defined, either as a default or when the specific resource type instance is created, the hyperlink label is not visible in
e
Procedure
.
TIP: The
Hyperlink descriptors and defaults
area is only accessible if, from the
General
tab, you selected the
Enable FactoryTalk eProcedure
option. Refer to the for more hyperlink information.
You can define up to five hyperlinks per resource type.
Define hyperlinks
  1. Open
    FactoryTalk Administration Console
    and sign into the
    FactoryTalk
    Network Directory.
  2. In
    FactoryTalk Administration Console
    Explorer
    , do one of the following:
    • For a new
      FactoryTalk Batch
      Server, right-click the application or the area name and select
      Add New Server
      FactoryTalk Batch Server
      .
    • For an existing
      FactoryTalk Batch
      Server, expand the application or the area name, right-click the server, and select
      Properties
      .
  3. In the
    FactoryTalk Batch Services Properties
    dialog, select the
    Descriptors and Defaults
    tab.
  4. In the
    Hyperlink descriptors and defaults
    area,
    Resource types
    dropdown list, select the appropriate type (
    Phase
    ,
    Process Cell
    ,
    Resource
    , or
    Unit
    ).
  5. In the
    Descriptors
    area, enter up to five hyperlink URL labels for the selected
    Resource type
    .
  6. In the
    Default values
    area, enter the default hyperlink URL associated with each defined
    Descriptor
    .
  7. Select
    Apply
    to save the data in the
    Descriptors and Defaults
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal