Add a FactoryTalk Batch Server
Add and configure a
FactoryTalk® Batch
Server, including FactoryTalk
Archiver properties, using the FactoryTalk Batch Services
Properties
dialog in FactoryTalk Administration Console
.
TIP:
For
FactoryTalk Batch
version 17.00 and
earlier, continue to configure the FactoryTalk Batch
Server, including associated
FactoryTalk
Archiver properties, using the Server
Options
dialog in FactoryTalk Batch Equipment Editor
.The configuration information for the
Configure
FactoryTalk Batch
Server provides centralized configuration for how
batch services operate. This includes configuration information for the location
of project files, restart behavior, event journal location and format,
miscellaneous runtime settings, and setting up archiving and reporting.FactoryTalk
Archiver properties to specify if and how electronic batch
record files (.evt
or .evtj
) are inserted into the
ODBC-compliant database.Changes to items such as
FactoryTalk Batch
Server properties, the area model
directory, and the error logging directory take effect after a FactoryTalk Batch
Server restart. Changes to the recipe directory or journal directory also require a FactoryTalk Batch
Server restart.Changes to
FactoryTalk
Archiver properties do not require a FactoryTalk Batch
Server restart. These changes take effect the next time the FactoryTalk Batch
Server needs the property.
TIP:
FactoryTalk Batch
does not support the use of mapped drives. Do not use mapped
drives for project directories.Prerequisites
Adding a
FactoryTalk Batch
Server requires these permissions for the application
or area:- Common > Create Children
- Common > Write
- Common > Read
To add a
FactoryTalk Batch
Server- OpenFactoryTalk Administration Consoleand sign in to theFactoryTalkNetwork Directory.
- InFactoryTalk Administration ConsoleExplorer, right-click the application or the area name.
- Select .
- On theGeneraltab, set up a primaryFactoryTalk BatchServer:
- In theNamebox, enter a label for theFactoryTalk BatchServer object.
- UseBrowseto locate the computer hosting the server.
- Configure server options.
- SelectApply.
- TIP: If either theEnable FactoryTalk eProcedureor theEnable FactoryTalk Batch Material Managercheckbox is selected, and theFactoryTalk Batch ViewServer is running, restart theFactoryTalk Batch ViewServer.
- On theProject Settingstab, configure the project paths. To save your changes, selectApply.
- On theBatch Reportingtab, configure the method and settings thatFactoryTalkArchiver will use to archive batch record data. To save your changes, selectApply.
- On theArchived Eventstab, configure the event types thatFactoryTalkArchiver will archive. To save your changes, selectApply.
- On theDescriptors and Defaultstab, set up Cross Invocation strings and hyperlinks. To save your changes, selectApply.
- (optional) On theAdvancedtab, set upFactoryTalk BatchServer extended properties. To save your changes, selectApply.
- (optional) Configure a secondaryFactoryTalk BatchServer to create aFactoryTalk BatchServer pair that can resume or continue batch execution on the other member of the pair.
- On theSecondary Servertab, set up a secondaryFactoryTalk BatchServer. To save your changes, selectApply.
- On theProject Settingstab, configure the project paths. To save your changes, selectApply.
- When finished, selectOK.
Provide Feedback