FactoryTalk Batch Services Properties dialog—General tab
In the
FactoryTalk Batch Services Properties
dialog, use the
General
tab to configure primary FactoryTalk® Batch
Server options.General tab settings
The
General
tab allows you to set up a primary FactoryTalk Batch
Server and configure server options.Setting | Description |
|---|---|
Name | Label in the FactoryTalk Directory for the FactoryTalk Batch Server object. Each
Name must be unique within a FactoryTalk Directory
application or area.Other specifications for this required field include:
|
Computer hosting the primary FactoryTalk Batch
Server | Browse to or enter the name of the host computer where the
primary FactoryTalk Batch Server resides.The host computer name can only be used by one FactoryTalk Batch Server object in the FactoryTalk Directory —not any
other primary or secondary FactoryTalk Batch Server (if
a secondary is configured). If you enter the same host computer
name for more than one FactoryTalk Batch Server object
in the FactoryTalk Directory ,
FactoryTalk Batch will use the configuration of the
FactoryTalk Batch Server object associated with the
first instance it finds of the host computer name.
TIP:
Automated validation for
uniqueness of the
FactoryTalk Batch Server computer
assignment does not run during FactoryTalk Directory
backup and restore of an individual application, so you must
verify the configuration to avoid anomalous behavior. |
Enable FactoryTalk
e Procedure | Select this option to specify that the FactoryTalk Batch
Server must work in coordination with FactoryTalk
e Procedure®
FactoryTalk
e Procedure®
FactoryTalk Batch Services Properties
dialog. |
Enable FactoryTalk Batch
Material Manager | Select this option to specify that the FactoryTalk Batch
Server must work in coordination with FactoryTalk Batch
Material Manager and enable FactoryTalk Batch
Material Manager options throughout the
FactoryTalk Batch Services Properties
dialog. |
TIP:
If either the
Enable FactoryTalk
eProcedure
or the Enable FactoryTalk Batch Material
Manager
checkbox is selected, and the FactoryTalk Batch View
Server is running, restart the FactoryTalk Batch View
Server.Batch creation
In the
Batch creation
area, configure how the primary FactoryTalk Batch
Server generates a unique ID for each batch at batch
creation, and the default batch name that the operator sees when adding a batch.Setting | Description |
|---|---|
Create ID range | For the purpose of batch identification, the primary FactoryTalk Batch Server generates a unique
CreateID for each batch at batch
creation. This Create ID range field controls the
range of IDs that the primary FactoryTalk Batch Server
can use when generating a CreateID . To
make sure that all IDs generated by a FactoryTalk Batch
Server pair are unique, you cannot select the same range for
both the primary FactoryTalk Batch Server and its
secondary server.
TIP:
The properties for the
Create ID range field for the
secondary FactoryTalk Batch Server are in the
Secondary Server tab. For more
information, see FactoryTalk Batch Services Properties dialog—Secondary Server tab.To generate a new CreateID , the primary
FactoryTalk Batch Server increments the last
CreateID by one (skipping any IDs
that exist in the eventdir.txt file). |
Default Batch ID | When adding a batch, one of the properties that the operator sees
in the FactoryTalk Batch View
Batch Creation page is the
Batch ID . This Default
Batch ID field defines the default value that
the operator initially sees in the Batch
ID property.The value in the Default Batch ID field
must meet the following requirements:
The default value for this required field is
BATCH_ID . |
Event files
During batch execution, the primary
FactoryTalk Batch
Server creates an
electronic batch record. An electronic batch record includes a complete record of
events for one batch. The Event files
area allows you to
configure settings related to the electronic batch record.Setting | Description |
|---|---|
File format | Define the file format of electronic batch records. Select one of
the following from the list:
|
Enable Event Journal Signatures | Select this option to turn on Event Journal Signatures, a
function that detects unauthorized changes to electronic batch
records ( .evt or .evtj
files).
TIP:
Refer to the
for
more information about Event Journal Signatures.
|
Miscellaneous
The
Miscellaneous
area allows you to define options for hold
propagation and limits.When a batch executing in a primary
FactoryTalk Batch
Server detects a
failure condition, the system may hold all or parts of a batch from propagating
through the recipe hierarchy. The selected Hold propagation
type identifies how much of the batch is commanded to hold in response to the
failure and how much continues to
run.Type | Description |
|---|---|
None | No hold. The entire batch continues running. |
Phase | Holds only the affected phase, allowing the balance of the
phase’s unit and all other units to continue running. |
Operation | Holds only the affected phase and the related operation, allowing
the balance of the operation’s unit and all other units to continue
running. |
Unit | Holds the phase and the related unit, and all other units
continue running. |
Batch | Holds the entire batch. This is the default value. |
Other settings in the
Miscellaneous
area allow you to define
options relating to limits.Setting | Description |
|---|---|
Maximum log file size (MB) | The primary FactoryTalk Batch Server logs activities to
a log file (Batchsvr.log ). This required
field defines the maximum size (in megabytes) of the log file.
When the log file reaches maximum size, the log acts in a
circular manner, with new records overwriting the oldest
records.This field has a minimum integer value of 1 and a maximum integer
value of 1,024. The default value is 10
MB. |
Minimum disk space (MB) | This required field defines the minimum disk space (in MB) that
must be available before a batch can be added to the
BatchList . Adequate disk space helps
prevent data loss.This field has a minimum integer value of 1 and a maximum integer
value of 1,024. The default value is 1
MB. |
Maximum number of items to verify in parallel | From the FactoryTalk Batch Service Manager , you can issue a runtime command to the primary
FactoryTalk Batch Server to verify tags in the area
model. Because attempting to verify all the tags simultaneously
can put a large load on the data servers supporting those tags,
and the customer could be running batches, by default the
command verifies one tag at a time.This required field allows you to increase the number of tags
that the command verifies at the same time, up to a maximum
integer value of 30. The default value is
1 . |
Minimum free virtual memory (MB) | This required field defines the minimum amount of virtual memory
(in MB) that must be available before the primary FactoryTalk Batch Server will allow batch creation.
Adequate memory helps prevent FactoryTalk Batch Server
crashes.This field has a minimum integer value of 102 and a maximum
integer value of 3,840. The default value is
512 MB. |
OPC communications timeout
The
OPC communications timeout
area allows you to configure
the primary FactoryTalk Batch
Server’s watchdog timer.Setting | Description |
|---|---|
Period (msec) | This required field defines the time interval (in milliseconds)
that the primary FactoryTalk Batch Server uses to check
the quality of communication with FactoryTalk Live Data servers and OPC data servers and
to attempt to reconnect logic in the case of lost data server
connections.This field has a minimum integer value of 1,000 and a maximum
integer value of 60,000. The default value is
10,000 msec. |
Allowable failures | This required field defines how many consecutive failed watchdog
set or reset periods that the primary FactoryTalk Batch
Server permits before a FactoryTalk Live Data server or OPC data server connection status
is marked BAD and batches using that data server respond
according to their configured Hold
propagation type.This field has a minimum integer value of 2 and a maximum integer
value of 999,999,999. The default value is
5 . |
Material policies
The
Material policies
area is only accessible when you select
the Enable FactoryTalk Batch Material Manager
option on this
tab. This area allows you to set up a FactoryTalk Batch
Material Manager
Server and configure FactoryTalk Batch
Server
behavior in the event of communication loss with the FactoryTalk Batch
Material Server.Setting | Description |
|---|---|
Computer hosting the FactoryTalk Batch Material
Server | Browse to or enter the path to the computer where the primary FactoryTalk Batch Material Server resides. The computer
must be in the FactoryTalk Directory . |
Communications lost behavior | Configure the behavior when the FactoryTalk Batch Server
loses communication with the FactoryTalk Batch Material
Server. Select one of the following options from the list:
|
Hold on Split Feed | This option, which is enabled by default, holds batches in the
event of a split feed.
TIP:
If you choose to disable this
option, batches may not get the expected material amounts unless
you create material loops in the recipe for every enabled
material. For information about using the
Create
Material Loop command, refer to the FactoryTalk Batch Recipe
Editor User Manual , publication BATCH-UM006 |
Provide Feedback