Triggers
A trigger is a set of criteria that, when met, starts the execution of one or more actions assigned in a task with the trigger. A given task can be started by one or more triggers. A workstation can have a maximum of 100 triggers.
FactoryTalk Action Manager
supports the following trigger types:- Date Time Based Triggers
- Windows Task Event Triggers
To create a trigger, select
or
Triggers
in the project view on the left, then select
or Create trigger
.To change the type of the trigger, select another type in
Type
.To delete a trigger, hover over a trigger and select
.
.Provide Feedback