Configure a Date Time Based Trigger
Date Time Based Trigger
starts actions within the same task at the specified times. This includes starting the task once at a specific time or starting the task multiple times on an hourly, daily, weekly, monthly on a specific day, or monthly day-of-week schedule.To configure a Date Time Based Trigger
- InType, selectDate Time Based Trigger.
- InTrigger Recurrence, configureStart dateandStart time.
- Select one of the recurrences:
- Hourly
- Daily
- Weekly
- MonthlyTIP:
- Select the recurrenceEvery 12 monthsto configure a yearly trigger.
- To configure updates forDaylight Savings Time(DST) changes, create two triggers using the start date and time when clocks are moved ahead or behind by one hour and configure the triggers to repeat every 12 months. For example, on the second Sunday in March or November. For more information, see Configure the Device Wall-clock Updates for Daylight Saving Time.
- ConfigureEnd date. If leftEnd dateblank, this trigger will occur without ending.TIP:After changing the system clock or time zone on the server computer, save the configuration to make your changes take effect.
Provide Feedback