Actions

An action defines an operation that is performed when a task detects that a trigger's criteria are met. A workstation can have a maximum of 100 actions.
FactoryTalk Action Manager
supports the following action type:
  • Device Wall-clock Update
To create an action, select
Actions
in the project view on the left, and then select Add button or
Create action
.
To check how this action is performed, select
Run
beside the action name.
To delete an action, hover over the action and select Delete button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal