Device Wall-clock Update action properties
The following table describes the settings of the Device Wall-clock Update action.
Item | Description |
|---|---|
Add | Adds devices by browsing in FactoryTalk Linx Network Browser or manually
entering device paths. You can add a maximum of 1000 devices to one action. |
Delete | Deletes the selected devices. Tip:
|
Online Status | Checks the status of the selected devices in the Device Status dialog box. |
Wall-Clock Update | Transfers the workstation wall-clock to the wall-clock of the selected devices. |
Import | Imports devices from a CSV file. The imported content will overwrite the existing content. |
Export | Exports all devices and their information in this list to a CSV file. |
Advanced Settings | Configures the advanced settings of the action in the Advanced Settings dialog box. |
Filter | Filters the devices using keywords. |
Properties table | Shows the device properties, including:
|
Provide Feedback