Synchronous Serial Interface (SSI) Encoder Type
One signed 32-bit position data is available on the module.
You configure the SSI mode in the Device Definition dialog in the Studio 5000 Logix
Designer application. For more information, see Device Definition.
Provide Feedback