PointMax Serial Module
The PointMax serial module provides an independent channel that functions as a network
interface to a wide variety of RS-232C, RS-422, and RS-485 devices. The channel can
transmit data to and receive data from serial devices using the following communication
mode:
- Generic ASCII
- Modbus Master
- Modbus Slave
Provide Feedback