Modbus Slave Data Exchange
For the Modbus Slave data exchange, the following definitions apply:
- Write – The Controller and Modbus Master can write data to the Modbus Slave.
- Read – The Modbus Master reads data from the Modbus Slave.
Modbus Slave Write Command
Modbus Slave Read Command
Provide Feedback