Control Line Menu

When you connect to a dial-up modem, see the following for details on duplex setting in a serial port.
Control Line Menu
Modem
Duplex Status
Controller
Function Choice
Continuous Carrier
Not using a modem
No handshaking
Using a modem
Modems in a point-to-point link are full-duplex.
Full-duplex
Modems in a point-to-point link are full-duplex.
Master controller
Full-duplex
Slave controller
Half-duplex
Select the continuous carrier checkbox.
All modems in a system are half-duplex.
Half-duplex
Clear the continuous carrier checkbox (default).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal