Field Power (SA Power) Loss Detection

The Field Power Loss Detection feature monitors the loss of field-side power on the SA power bus. In the diagnostic assembly, the
FieldPowerOff
bit is set at the module and channel level structure. The
Fault
bit is set at the channel level.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal