Retentivity storage methods
Retentivity storage objects expose Backup and Restore methods.
Backup
Use this method to back up the retentivity storage data to a file.
TIP:
You can track completed retentivity storage
backups with the Backup Completed event. See Backup Completed event.
Argument | Data type | Description |
|---|---|---|
OutputFilePath | String | Path to the file for retentivity storage backup in the
ResourceUri format. |
To implement the Backup method into your
FactoryTalk Optix Application
logic, see
Add a method to an existing event. For example,
add the Backup method to the MouseClick event of a button. See Configure retentivity storage backup and restore buttons.Restore
Use this method to restore the retentivity storage data from a backup file.
Argument | Data type | Description |
|---|---|---|
BackupFilePath | String | Path to a backup file to restore the retentivity storage data
from. |
To implement the Restore method into your
FactoryTalk Optix Application
logic,
see Add a method to an existing event. For example,
add the Restore method to the MouseClick event of a button. See Configure retentivity storage backup and restore buttons.Provide Feedback