Backup Completed event
Use Backup Completed event to track completed backups of retentivity storage
objects.
Operation
The Backup Completed event triggers when the Backup method of a retentivity storage
completes. See Retentivity storage methods: Backup.
Implementation
To implement the Backup Completed event into your
FactoryTalk Optix Application
logic, associate a method to execute when the Backup Completed event triggers. See
Add a method to an existing event.Result codes
The Backup Completed event can return the following codes.
Code | Description |
|---|---|
0 | Success |
1 | Store error |
2 | Empty filenames |
3 | Generic error |
Provide Feedback