Upload and register a device description file in the Network Browser
Upload and register device description files of devices within the .
FactoryTalk Linx
Network BrowserFor an online device in the network topology tree, if there is a device description file within the device's firmware, you can upload the device description file in the and register it to the , and communications to other information within the device are possible.
FactoryTalk Linx
Network BrowserFactoryTalk Linx
data server. Once registered, the device information shows in the FactoryTalk Linx
Network BrowserUse the to:
FactoryTalk Linx
Network Browser- Manually upload and register a device description file
- Automatically upload and register a device description file
Fournir une réponse