Register device description files using the Device Description File Installation Tool
You can register the device description files of hardware devices, including EDS and IODD files, by launching the
Device Description File Installation Tool
.Before you begin:
- To register the device description file of a hardware device, you must have a valid and complete device description file of the hardware device. To search and download the device description file of a specific hardware device, visitRockwell AutomationNetwork Resources.
- If an icon file (*.ico) exists for the hardware device, save it with the same name as the device description file in the same directory. You can save one or more device description files (and the related icon files) in one directory.
To register device description files using the Device Description File Installation Tool
- From the WindowsStartmenu, selectAll Programs >.Rockwell Automation> RSLinx > Tools > Device Description File Installation Tool
- In theDevice Description File Installation Tooldialog box, clickAdd. TheDevice Description File Installation Tooldialog box opens.
- In theRegistrationdialog box:
- SelectRegister a single device description fileto register one device description file at a time, or
- SelectRegister a directory of device description filesto register two or more device description files at a time.
- In theRegistrationdialog box, clickBrowseto select the device description file (if you are registering a single file), or the directory of the device description files (if you are registering two or more device description files), and clickNext.
- In theDevice Description File Installation Test Resultsdialog box, review the hardware device list and clickNext.
- In theChange Graphic Imagedialog box, review the icons of the hardware devices and clickNext.CONSEIL:Device Description File Installation Tool assigns a default icon to each hardware device. You can specify a different icon for the hardware devices by selecting the hardware device and clicking theChange iconbutton.
- In theFinal Task summarydialog box, review the hardware device list and clickNext.
- When the registration is completed, clickFinishto return to theDevice Description File Installation Tooldialog box.
- ClickExit.
Fournir une réponse