Configure Safety I/O Devices
Add the safety I/O device to the communication device in the I/O configuration of the controller project.
TIP:
Some safety I/O devices support both standard and safety data. The device definition settings define what data is available.
- Right-click the Ethernet network and select New Module.

- On the Select Module Type dialog box, select the safety I/O device and click Create.TIP:Use the filters to reduce the list of devices to choose from.

- Enter a name and IP address for the new device. If your network uses Network Address Translation (NAT), see Use Network Address Translation (NAT) with CIP Safety Devices.

- To modify the module definition settings, click Change.IMPORTANT:For safety I/O devices, do not use Disable Keying. See Electronic Keying.
- To modify the safety network number, click the ellipsis button.
- Set the connection reaction time limit by using the Safety tab.For information about system reaction time, see the GuardLogix 5580 and Compact GuardLogix 5380 Safety Reference Manual, publication 1756-RM012.
- To complete configuration of the safety I/O device, refer to the user documentation and the Logix Designer online help.
Provide Feedback