Requirements for Use Control
Security Component | Required to Meet IEC-62443-4-2 SL 1 | Details |
|---|---|---|
Studio 5000 Logix Designer® application | May be required based on system design, threat model, and risk assessment. | Configure the controller project in the Logix Designer application to use these user access methods:
For more information, see Logix 5000 Controllers Security Programming Manual, 1756-PM016 . |
FactoryTalk® Security softwareStudio 5000 Logix Designer® application | Yes | Configure FactoryTalk® Security to define policies, user groups, and other permission sets.
For more information, see Configure System Security Features User Manual, SECURE-UM001 . |
Controller keyswitch position | May be required based on system design, threat model, and risk assessment. | Place the keyswitch in the RUN position to help prevent unauthorized remote configuration changes to the controller, and restrict some communication services. Remove the keyswitch from a running controller to help prevent modifications to the configuration or program. IMPORTANT: Do not apply a new security policy while the controller is in RUN mode. RUN mode does not help prevent updates to the security policy, and a policy change has the potential to disrupt a running control system. |
Disable the controller Ethernet port | May be required based on system design, threat model, and risk assessment. | The Ethernet port is enabled by default. Disable the Ethernet port if required by the system design, threat model, or risk assessment. For more information, see Disable the Ethernet Port on the Port Configuration Tab and Disable the Ethernet Port with an MSG Instruction. |
Disable Simple Network Management Protocol (SNMP) on the controller (firmware revision 32 or later) | May be required based on system design, threat model, and risk assessment. | SNMP is disabled by default. If SNMP has been enabled, disable SNMP if required by the system design, threat model, or risk assessment. For more information, see Use a CIP Generic MSG to Disable SNMP on the Controller. |
Disable the controller CIP Security™ ports | May be required based on system design, threat model, and risk assessment. | CIP Security™ ports on the controller are enabled by default. Disable the CIP Security™ CIP Security™ ports if required by the system design, threat model, or risk assessment.For more information, see Disable CIP Security Ports via FactoryTalk Linx and Disable CIP Security Ports via a CIP Generic MSG Instruction. |
Disable the controller USB ports | May be required based on system design, threat model, and risk assessment. | The USB port on the controller is enabled by default. Disable the USB port if required by the system design, threat model, or risk assessment. For more information, see Disable the Controller USB Port. |
Disable the controller SD card | May be required based on system design, threat model, and risk assessment. | The SD card is enabled by default. Disable the SD card if required by the system design, threat model, or risk assessment. For more information, see Disable the Controller SD Card. |
Disable controller webpages | May be required based on system design, threat model, and risk assessment. | Controller webpages for diagnostics are read-only. With Studio 5000 Logix Designer® application version 33 or later, controller webpages are disabled by default. Disable the controller webpages if required by the system design, threat model, or risk assessment.For more information, see Disable Controller Web Pages. |
Provide Feedback