Popup tab
How do I open the Popup tab?
In the
.
Project Explorer
, expand the User-Defined Screens
folder, and double-click a popup. Popup names are preceded by a Popup
icon Use the
Popup
tab to view and modify the contents of a superimposed window to appear on a screen on the HMI device. A popup can show additional information for the open screen or a prompt to perform a task. Popups open when an event configured with an Open Popup
command triggers. Use the
Popup
tab to: - Change the caption of a popup.
- Insert and configure graphic elements on the popup like any other screen.
Provide Feedback