Popup contents
A popup is a small window superimposed on a screen. A popup has basic components:

Item | Description |
![]() | An optional caption describing the contents and data the popup contains. On the HMI device, move a popup by dragging the caption. If a popup does not have a caption, the popup cannot move on the HMI device. |
![]() | An optional Close button. Select Close to close the popup on the HMI device. Other methods of closing popups include selecting elsewhere on the screen, opening the Navigation menu , opening another screen or popup, or creating an event with a Popup Close command. |
![]() | The contents of the popup. |
Provide Feedback