Users tab

How do I open the Users tab?
On the
Menu
bar, click
Tools > Security Administration
, and from the
Security Administration
dialog box, click the
Users
tab.
Use the
Users
tab on the
Security Administration
dialog box to:
  • Create, delete, or sort user accounts for each person who interacts with the HMI device.
  • Assign the password and/or PIN for users to log on to the HMI device.
  • Assign a role to each user.
  • Change the default role of the Guest user. None grants the Guest user access to the
    Home
    screen only. Any non-Administrator role, including None, prevents any non-Administrator user from changing settings on the HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal