Security roles

In
View Designer
security, a user is comparable to a Windows user account, and a role is comparable to a Windows user group. No specific behavior is assigned to each role.
Assign a role to each user on the
Security Administration > Users
tab. The assigned role determines which screens the users in the role can access according to the security settings for the screens. All users have the
Operator
role by default.
The
View Designer
roles to assign to users include:
Role
Responsibility
Administrator
Administering the system, such as adding users and assigning passwords. This security role is assigned to Guest users by default.
Engineer
Automating the machine and creating or setting the direction of the HMI.
Maintenance
Keeping the system running at maximum efficiency, and using the HMI screens to troubleshoot, diagnose, and maintain equipment.
Operator
Running the machine or process, and using the HMI project to view and interact with the process. This security role is assigned to new users by default.
Restricted
Activities requiring less access than an
Operator
. Determine screen access based on business needs. This role prevents any non-Administrator user from changing settings on the HMI device.
Supervisor
Overall production of the machine or plant and uses the HMI screens for critical information, such as the product production, production rate, downtime, and product quality.
None
Indicates that no role is associated with the
Guest
user. This option is available for the
Guest
user account only. Assigning this role grants the
Guest
user access to only the
Home
screen.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal