Add a Security Administration user account
To control user access to the runtime application at different levels, create a user account for every person that will interact with the HMI Device. Assign a security role and password and/or PIN to each user. It is recommended to define no more than 500 users.
To add a Security Administration user account
- SelectTools > Security Administrationand select theUserstab.
- SelectAdd user
or start typing in the last user card to create a new user card.TIP:Typing in theUser Namebox opens a card for data entry. - In theUser Namebox, type the name that the user will use to log on to the HMI device. This name displays in the banner on the HMI device.TIP:Tips:
- The name can contain up to 40 characters of numbers, letters, and underscores.
- The name must not begin with a number, contain spaces, have more than one underscore in a row, or end with an underscore.
- TheUser Namebox cannot contain Unicode characters.
- (optional) In theFull Namebox, type the first and last name, up to 100 characters, of the user.
- (optional) In theDescriptionbox, type a description, up to 100 characters, of the user.
- In theRolebox, select the security role to assign to the user.
- Enter and confirm the password and/or PIN the user will use to log on to the HMI device.
- Passwords must adhere to the policies you configured on thePoliciestab on theSecurity Administrationdialog box.
- PINs must have a minimum of four numbers and a maximum of eight numbers.
- IfPassword Must Meet Security Requirementsis selected onPoliciestab, passwords must meet complexity requirements.
- Passwords can contain Unicode characters.TIP:To meet complexity requirements, passwords must:
- Not contain the User Name.
- Not contain any portion of the Full Name.
- Contain characters from three of the four following categories:
- Uppercase characters of European languages (A through Z, with diacritic marks, Greek and Cyrillic characters)
- Lowercase characters of European languages (a through z, sharp-s, with diacritic marks, Greek and Cyrillic characters)
- Numbers 0 through 9
- Non-alphanumeric characters ~!@#$%^&*_-+=`|\(){}[]:;"'<>,.?/
- SelectOKto save the changes and close theSecurity Administrationdialog box, or selectAdd User
to continue adding users.TIP:Tips:- Copy and pasteSecurity Administrationuser accounts from otherView Designerprojects to save time.
- To reset the password for a user, selectReseton the account card for that user.
Provide Feedback