Upload a runtime application from an HMI device

Use the
Upload Runtime Application
wizard to transfer a runtime application from an HMI device to a computer.
In the wizard, specify the communication path between the HMI device and the computer to which it will be uploaded and then specify where you want to save the uploaded runtime application file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal