Upload and save a runtime application
Use the
Upload Runtime Application
wizard to transfer a runtime application from an HMI device to a computer. Perform the transfer if the .VPD project file no longer exists on the computer that is running View Designer
. This allows making further changes to the project and downloading the project to the HMI device again.
IMPORTANT:
Runtime applications contain a .vpd extension. Downloading a file without a .vpd extension to an HMI device is not supported.
To upload and save a runtime application:
- On theMenubar, clickCommunications > Uploadto start theUpload Runtime Applicationwizard.
- In theHMI Device Pathbox on theHMI Device Locationpage, select the IP address of the HMI device containing the runtime application:
- Click the arrow to select a previously used path.
- ClickBrowse
and select the HMI device.
- ClickUpload. TheHMI Device Locationpage displays the progress of the upload process.
- If a problem exists, an error message displays at the point it occurred and the process stops. Resolve all of the errors before uploading the runtime application.
- When the upload is complete, clickSave.
- In theProject Filebox on theSavepage, select the location to save the file:
- ClickBrowse
to navigate to the location. - Type the path in theProject Filebox.
- ClickSave.
- WhenFinishedis selected to indicate the process is complete, clickClose.TIP:The first time using theUpload Runtime Applicationwizard, theHMI Device Pathbox is blank. On subsequent use of the wizard, theHMI Device Pathdefaults to the most recent IP address that was used successfully.
Provide Feedback