Automatic Diagnostics

View Designer
has an Automatic Diagnostics lists that displays the diagnostics in a project or configured HMI device. Each project contains an
Automatic Diagnostics
screen by default. Create an additional screen with an Automatic Diagnostics graphic element to create a custom
Automatic Diagnostics
screen.
Diagnostics in the project have the status of either
Active
or
Inactive, Suppressed
. View the
Details
pane of the
Automatic Diagnostics
screen to see data such as Message, Event Time, Diagnostic Code.
Use automatic diagnostics on an HMI device to:
  • Suppress a diagnostic.
  • Unsuppress a diagnostic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal