Details pane for Automatic Diagnostics
Select
on an automatic diagnostics table to open the
Details
on an automatic diagnostics table to open the Details
pane.In a medium Automatic Diagnostics table intended for HMI devices with seven- to nine-inch screens, the
Details
pane replaces the list of automatic diagnostics in the table. In a large Automatic Diagnostics table intended for HMI devices with ten-inch or larger screens, the Details
pane opens at bottom of the automatic diagnostics table.

NOTE:
The
Details
pane with additional details for the selected automatic diagnostics. This pane displays data, such as Message, Event Time, Diagnostic Code. When multiple diagnostics are selected, details display for the last selected automatic diagnostics. The contents of the
Details
pane appears in rows.Row | Description |
|---|---|
Message | The message with a fault description. |
Device Name | The name of the controller for which automatic diagnostics occurred. |
Product Name | The name of the Rockwell Automation application for which automatic diagnostics occurred. |
Event Time | The date and time the automatic diagnostics event occurred. |
State | The state of an automatic diagnostic. |
Diagnostics Code | The message defining what type of diagnostics occurred. |
Resource | The resource that reports a fault. |
Catalog | The device catalog number. |
Product Type | The type of a product that provides detailed information about the device that reports a fault. |
Vendor | The vendor of a device that reports a fault. |
Version | The firmware version of a device for which automatic diagnostics are reported. |
Provide Feedback