Open Project dialog box

How do I open the Open Project dialog box?
On the
Menu
bar, click
File > Open project
. The
Open project
option is also available on the
Studio 5000
Launcher.
The
Open Project
dialog box provides a list of HMI projects saved to the computer. Use the
Open Project
dialog box to select and open a project.
Close any open project before opening another project. Projects in other instances of
View Designer
may remain open. It is recommended that no more than three instances of
View Designer
run at one time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal