Save a copy of a project
Use the
Save Project As
command to create a copy of an open project. Create a copy of a project to: - Create a project from an existing project.
- Prevent overwriting the original project.
To save a copy of a project
- SelectFile > Save Project As.
- In theFile namebox, type a name for the project.
- SelectSave. The open project is now the new project, not the original project. Pending edits are saved only to the new project. They are not saved to the original project.TIP:View Designercannot save a project if a .vpd file with the same name is open in another instance ofView Designer.
- (optional) Rename the project.
Provide Feedback