Information Attributes

Create custom Information Attributes.
You can apply Information Attributes to any element in the information model including models, nodes, and properties.
An Information Attribute can have a value or be a flag only. A flag only attribute is applied to the model element or not applied, depending on the toggle.
Information Attributes names are a string of up to 40 alphanumeric characters. The only allowed special characters are space, underscore, and dash. The name cannot start or end with a space, and cannot be blank.
Each Information Attribute must be unique.
A predefined list of Attributes is included in your system. The prefix for Rockwell Information attributes is raC, and you can install attributes with this prefix. You can organize Information Attributes in categories, or export and import the list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal