Map FactoryTalk Smart Object properties to a ThingWorx template or shape

When a node uses a ThingWorx template or shape, by default, the properties of the node (DINT, REAL, LINT, STRING) map to properties inherited from the ThingWorx template or shape.
If the node uses a ThingWorx template or shape but contains properties that are not in the ThingWorx template or shape, Smart Object Configurator creates the corresponding properties on the target Thing.
To map
FactoryTalk Smart Object
properties to a ThingWorx template or shape
  • In
    The parent node for this property uses a ThingWorx template. Map property value to a
    , select:
    Template or Shape property
    : Maps the value to properties inherited from a template or shape property. This is the default behavior.
    You can add single template and maximum 5 shapes.
    TIP:
    The data type and property name in both
    FactoryTalk Smart Object
    and the template property must match.
Thing property
: Maps the
FactoryTalk Smart Object
property to a new Thing property in ThingWorx Composer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal