What is FactoryTalk View File Viewer?
Use
FactoryTalk View
File Viewer to view the following types of log files:- SE data log files
- ME data log files
- ME alarm log files
- dBase files
- ME RecipePlus files
- SE RecipePro file
The log information can be shown in the form of list views or trend plots. You can save the files as CSV list, CSV table, or dBase files so that it is easier to do more analysis.
FactoryTalk View File Viewer only works on computers with Microsoft Windows operating systems. To view ME files from PanelView Plus CE or PanelView Plus terminals, you can copy the files to a CompactFlash (CF) or Secure Digital (SD) card and move them to the computer where the utility resides.
TIP:
Before opening the log files, make sure that you stop the running
FactoryTalk View ME
application or FactoryTalk View SE
data log.Provide Feedback