View FactoryTalk View log files
After opening a
FactoryTalk View
log file, you can view the information in a list or plot window.To view
FactoryTalk View
log files- SelectFile>Openor select
on the toolbar. - In theOpendialog box, select the log file type.
- Select the file you want to view and clickOK. The log appears in a list view window.
- If you view ME data log files or ME alarm log files, complete these steps:
- View ME data log filesIn theSet Time Zonedialog box, select a time zone that you want the date time information to be converted in, and clickOK.The conversion starts and the progress shows in theConverting Log file to dBase filedialog box.
- View ME alarm log filesIn theSelect RSView ME Alarm Setup Filedialog box:
- From the terminal list, select an option to specify where the log file is generated.
- ClickBrowseto select the ME setup file (*.mal).TIP:Only use the .mal file that comes from the HMI project directory. Using a runtime .mal file may result in missing theMessagecolumn information.The file is located in\Users\Public\Documents\RSView Enterprise\ME\HMI projects\<App_Name>\M_Alarms\
- To view the log file in a trend plot window, selectView > Plotor click
on the toolbar.
Provide Feedback