Set up data log triggers

Use the
Log Triggers
tab to set up how data logging is triggered. The default is
Periodic
logging every 10 seconds. This automatically logs the values of the tags in the data log model every 10 seconds.
To set up data log triggers:
  1. In the
    Data Log Model
    editor, click the
    Log Triggers
    tab.
  2. To to log tag values periodically, select
    Periodic
    .
  3. To only log tags whose values have changed, select
    On Change
    .
  4. To log tag values when the FactoryTalk View command
    DataLogSnapshot
    is issued, select
    On Demand
    .
    TIP:
    The data log model must be running before the
    DataLogSnapshot
    command is given.
    When you select
    On Demand
    logging, tags are logged when the
    DataLogOn
    and
    DataLogOff
    commands are issued, as well as when the
    DataLogSnapshot
    command is issued.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal