Data Log Models editor - Log Triggers tab
The following table shows options in the tab if you select
Periodic
.Option | Description |
|---|---|
Periodic | Select this option to log tag values periodically. |
Interval | Type a number and select a time unit to specify how often tag values are logged. All tags are logged each time this interval expires.
|
The following table shows options in the tab if you select
On Change
.Option | Description |
|---|---|
On Change | Select this option to only log tags whose values have changed. Use the On Change trigger to log tag values after a certain percentage of change in the value occurs. The percentage is based on the tag's minimum and maximum (or High EU and Low EU) values. For example, if you specify 10, a tag's value must change by 10 percent before it is logged. This applies to analog HMI tags only. For data server tags, and digital and string HMI tags, which do not have minimum and maximum properties, every change is logged. |
Maximum Update Rate | Click an item in the seconds list to select the maximum rate at which tags in the data log model are updated. The default maximum rate at which tags are updated is 1 second. |
Change Percentage | Type the percent a tag value must change to trigger logging. Zero means all changes are logged. The change percentage can contain decimals. |
Heartbeat | Type a time and click a time unit to specify how often tag values are logged even if no change has occurred. The heartbeat ensures that the data in the log file is current. The heartbeat rate must be equal to, or greater than, the update rate. Specify 0 for the heartbeat if you do not want to use it. Tag values will be logged only when they change. |
The following table shows options in the tab if you select
On Demand
.Option | Description |
|---|---|
On Demand | Select this option to log tag values when the FactoryTalk View command DataLogSnapshot is issued.This command can issued anywhere that other FactoryTalk View commands and macros can be. For example, you can type it in the command line, or specify it as the action for an event. If you specify Periodic or On Change , you can still use On Demand logging whenever it is appropriate. |
Maximum Update Rate | Click an item in the seconds list to select the maximum rate at which tags in the data log model are updated. The default maximum rate at which tags are updated is 1 second. |
Provide Feedback