Create a data log model
Use the
Data Log Models
editor to create a data log model.
TIP:
To use data in multiple formats, define multiple data log models for the same set of tags.
To create a data log model:
- In theData Log Modelseditor, in theSetuptab, type a description and log file identifier string and select a storage format.
- In thePathstab, specify the paths to the logging primary and secondary destinations.
- In theFile Managementtab, specify when the creation and deletion of files will take place.
- In theLog Triggerstab, specify how data logging will be triggered.
- In theTags in Modeltab, specify that tags will be logged.
- When complete, clickOK.
- When prompted, in theSavedialog box, type a name for the component and clickOK.
Provide Feedback