Runtime navigation
The way the operator moves between the graphic displays that make up the user interface in an application is referred to as navigation.
For the operator to navigate at runtime, do any of the following:
Provide Feedback