FactoryTalk View commands

In a
FactoryTalk View SE
application, you can use commands in:
  • Macros or symbols.
  • Command line.
  • Fields that require you to enter an action. For example, as the press, release, or repeat action when you assign touch animation to an object in a graphic display, or as the action for a button.
You can use the command line in the Command Line window of
FactoryTalk View Studio
.
On the
FactoryTalk View SE
Client,
FactoryTalk View
commands take precedence over macros. For example, if you have a macro called
Display
, the
Display
command will run whenever you try to run the
Display
macro.
In the command description, the following conventions are used:
  • Parameters enclosed in angle brackets
    <
    file
    >
    are required.
  • Parameters enclosed in square brackets
    [
    file
    ]
    are optional.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal