Alarms

Use
FactoryTalk Alarms and Events
as your alarming strategy. This alarming system allows multiple FactoryTalk products to share a common view of alarms and events throughout a FactoryTalk system. With
FactoryTalk Alarms and Events
, a
FactoryTalk View
application can include the following alarm monitoring:
  • Device-based alarms, including:
    • Logix instruction-based alarms
      Alarm instructions are programmed and then downloaded into the
      Studio 5000
      controllers. The controller detects alarm conditions and publishes the alarm information, which is routed to
      FactoryTalk Alarms and Events
      .
    • Logix tag-based alarms
      Logix tag-based alarms associate alarm conditions with tags for
      Studio 5000
      controllers. Logix tag-based alarms monitor tag values to determine the alarm condition, but they are not part of the logic program and do not increase the scan time for a project. Logix tag-based alarms are supported only on
      Compact GuardLogix
      5380,
      CompactLogix
      5380,
      CompactLogix
      5480,
      ControlLogix
      5580, and
      GuardLogix
      5580 controllers.
  • Server tag-based alarms
    Alarm conditions are defined and managed with software that monitors programmable controllers through tags. Tag-based alarm monitoring is supported by
    Rockwell Automation
    controllers communicating through
    Rockwell Automation
    device servers (
    FactoryTalk Linx
    ), third-party controllers communicating through OPC data servers, and HMI tags. Use server tag-based alarm monitoring if you do not want to use the pre-built instructions in Studio 5000 Logix Designer, or do not have Studio 5000 controllers.
  • OPC UA alarms
    Alarm conditions are provided by third-party OPC UA servers. The alarm data is then routed to
    FactoryTalk Alarms and Events
    through FactoryTalk Linx OPC UA Connector.
For complete information about using FactoryTalk alarms and events, see
FactoryTalk Alarms and Events Help
. For an example that uses alarm expressions to animate the color of a box when the state of an alarm changes, see
FactoryTalk Alarms and Events System Configuration Guide
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal