XML elements and attributes
An XML document can contain element types, elements, and attributes of elements. Each XML document has a single element called the document element or root element, which contains other nested elements. The root element of a graphic XML document is the
gfx
element. It represents the graphic display.Other elements defining and describing the graphic display are nested in the gfx element. Elements consist of a start-tag, the element's contents, and an end-tag. Elements have attributes, and attributes have values. You can specify multiple attributes for an element and have multiple elements in an XML file.
Elements can also have sub-elements nested within them, with their own attributes. Captions, imageSettings, states, animations, thresholds, and connections are examples of sub-elements. These in turn may have their own sub-elements, such as stateID elements within the states element, animateType elements within the animations element, threshold elements within the thresholds element, and connection elements within the connections element. caption and imageSettings elements can be sub-elements of a graphic object, or sub-elements within a state sub-element.
In the help definitions of elements and attributes:
- Text in quotes "" indicates a data type such as string, integer, float, and other.
- Text separated by a vertical bar | indicates the possible values for an attribute, only one of which can be specified at a time.
- Values appear in double quotes and follow an equal (=) sign.
Provide Feedback